Breakpoints
-
-
This feature is only available when you have chosen the DEBUG mode.
See click here... for more information.
- Breakpoints are a marker that is set in code which, when reached, stops the code's execution at that location. This lets you run one step further in the program with stepping commands.
-
-
Pausing a program does not interrupt the current VM cycle.
The current cycle finishes and execution is paused before the beginning of the next VM cycle. - Breakpoints are shown as a red circle (dark or light) in the left margin.
- Breakpoints may be active (
) or inactive (
).
- Breakpoints are active only when the IDE is connected to a target running an application that is compiled from the exact code displayed in the editor.
- Breakpoints are inactive if the IDE is:
- not connected to a target.
- connected but not running.
- connected to a different version of the code.
- connected to the code but a modification has been made in Edit mode.
- Breakpoints will always be applied to the target, based on their position in the editor. If a breakpoint is moved in the editor, then you reconnect to a target, the breakpoint in the target will be moved to the new position.
- A Breakpoint that has been "hit" has a yellow triangle (
and
) to indicate it has been reached in the code.
- Breakpoints are saved when saving the KAS application and are reloaded when loading a KAS application.
- See Setting, Removing, Enabling, and Disabling Breakpoints for information on working with breakpoints.
- See Breakpoints tab for information on the Breakpoints tab in the Information and Logs widget.
- Projects support a maximum of 16 breakpoints. This includes both enabled and disabled breakpoints.
-
-
Breakpoints can significantly increase the PLC cycle time execution. This is due to the fact that the VM must evaluate the breakpoint condition at every cycle.
Online Change
- Online Change cannot be enabled when the KAS Runtime is paused due to a breakpoint.
- Every breakpoint is activated if an Online Change is performed successfully.
-
-
The breakpoints are not activated synchronously but in a reasonable time.
- All breakpoints become inactive when an Online Change is reverted.