Device toolbar
This table describes each Device toolbar button.
|
Button |
Name |
Description |
|---|---|---|
|
Project Settings |
Click to open the Project Settings dialog box. |
|
|
Simulator |
Change the Controller IP address to connect with KAS Simulator. |
|
|
Compile project |
Compile the project. |
|
|
Compile and Download |
Compile and download the project. |
|
|
Connect |
Establish a connection with the target Controller. For possible statuses, see the Color Codes table for the labels of the status bar. |
|
|
Disconnect |
Close connection with the target Controller. |
|
|
Download |
Download the application to the targeted Controller (Note that the application must not be running). See Download the Project. |
|
|
Start |
It can be either a Warm or Cold start. |
|
|
Stop |
Stop the application. |
-
-
- The Allow Variables to be Locked option cannot be changed while the Online Change Enabled option is selected.
- If Online Change is enabled, deselect the Online Change Enable option first, enable or disable PLC Variable Locking, then re-enable Online Change, and re-compile the project.