FBD Variables
- Click this button in the FBD toolbar to insert a variable tag:
Insert variable: In this mode, the mouse is used for inserting variable tags.
Click in the diagram and drag the new variable to the desired position.
- Double-click a variable tag to open the variable selection box.
See Select FBD Variables and Instances for more information. - Either select the symbol of a variable or enter a constant expression.
Variables tags must be linked to other objects (e.g., block inputs and outputs) using connection lines. - Resize a variable box vertically to display, together with the variable name, its tag (short comment text), and its description text.
The variable name always appears at the bottom of the rectangle:
Display Item | Example |
---|---|
Description |
![]() |
Tag | |
Name |
See Variables tab for more information.