You are here: Technical References > Motion Library > Motion/Pipe Network > MLAxisInit

FunctionMLAxisInitPipe Network motion icon

Description

Initializes an axis object. Returns TRUE if the function succeeded

Arguments

Input

AxisID

Description

ID Name of the Axis block

 

Data type

DINT

 

Range

—

 

Unit

n/a

 

Default

—

ModuloPosition

Description

Value of the period of a cyclic system expressed in user units. The parameter is defined to correctly manage the periodicity (modulo) of the input values

 

Data type

LREAL

 

Range

—

 

Unit

User unit

 

Default

—

UserUnitPerTurn

Description

Define the unit which is equivalent to one revolution of the physical motor

 

Data type

LREAL

 

Range

—

 

Unit

n/a

 

Default

—

FeedbackUnitPerTurn

Description

 
 

Data type

DINT

 

Range

—

 

Unit

n/a

 

Default

—

Speed

Description

Sets the Axis Speed

 

Data type

LREAL

 

Range

—

 

Unit

User unit

 

Default

—

Acceleration

Description

Sets the Axis Acceleration value

 

Data type

LREAL

 

Range

—

 

Unit

User unit/sec2

 

Default

—

Deceleration

Description

Sets the Axis Deceleration value

 

Data type

LREAL

 

Range

—

 

Unit

User unit/sec2

 

Default

—

InitialPosition

Description

Initial position value expressed in user logical units. Used only at the pipe activation to initialize the position starting point

 

Data type

LREAL

 

Range

—

 

Unit

User unit

 

Default

—

Modulo

Description

Define the mode which can be Modulo (True) or not (False)

 

Data type

BOOL

 

Range

0, 1

 

Unit

n/a

 

Default

—

Output

Default (.Q)

Description

Returns true when function successfully executes

See more details here

 

Data type

BOOL

 

Unit

n/a

Example

Structured Text

MLAxisInit( PipeNetwork.Axis1, 360.0, 360.0, SHL(1,20), 500.0, 100000.0, 100000.0, 0.0, true ) ;

Ladder Diagram

MLAxisInit: LD example

 

Function Block Diagram

MLAxisInit: FBD example

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™