You are here: Technical References > Motion Library > Motion/Pipe Network > MLAxisPower

FunctionMLAxisPowerPipe Network motion icon

Description

Powers up or down the axis. EnableEnable signal for the drive, Hardware-Enable with 24V signal to X8, Software-Enable command by setup Software, fieldbus or permanently set. Both are required for enabling the drive. or disabled Axis Servo DriveA servo drive is a special electric amplifier used to power electric servo motors. It monitors feedback signals from the motor and continually adjusts for deviation from expected behavior.

When the axis is powered up, the ReferencePosition is modified to equal the ActualPosition. For that, KAS updates the GeneratorPosition. See About Associated Data on Positions for more information.

Arguments

Input

ID

Description

ID Name of the Axis block

 

Data type

DINT

 

Range

—

 

Unit

n/a

 

Default

—

On

Description

Flag to power up (True) or down (False) the Axis

 

Data type

BOOL

 

Range

0, 1

 

Unit

n/a

 

Default

—

Output

Default (.Q)

Description

Returns true when function successfully executes

See more details here

 

Data type

BOOL

 

Unit

n/a

Related Functions

MLAxisPowerDOff

Previous Function Name

MLAxisPowerOn

MLAxisPowerOff

Example

Structured Text

(* If Power_OnOff is TRUE then power in ON, otherwise OFF*)
MLAxisPower( PipeNetwork.Axis1, Power_OnOff) ;

Ladder Diagram

Function Block Diagram

MLAxisPower: FBD example

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™