You are here: Technical References > Motion Library > Motion/Pipe Network > MLAxisPowerDOff

FunctionMLAxisPowerDOffPipe Network motion icon

Description

Returns the adjustment of position done by the last power on to avoid bumps

Arguments

Input

ID

Description

ID Name of the Axis block

 

Data type

DINT

 

Range

—

 

Unit

n/a

 

Default

—

Output

Default (.Q)

Description

Returns true when function successfully executes

See more details here

 

Data type

BOOL

 

Unit

n/a

PowerONDeltaOffset

Description

 

Data type

LREAL

 

Unit

User unit

Related Functions

MLAxisPower

Example

Structured Text

 

Axis1_Power_On_Delta_Offset := MLAxisPowerDOff(PipeNetwork.Axis1 ) ;

 

Ladder Diagram

MLAxisPowerDOff: LD example

 

Function Block Diagram

MLAxisPowerDOff: FBD example

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™