| FunctionA function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. | Description |
|---|---|
| MC_GrpReadActAcc | Reads the actual acceleration of the group and the axes in the group. |
| MC_GrpReadActPos | Reads the actual position of the axes in the group. |
| MC_GrpReadActVel | Reads the actual velocity of the group and the axes in the group. |
| MC_GrpReadCmdPos | Reads the command position of the axes in the group. |
| MC_GrpReadCmdVel | Reads the command velocity of the axes in the group and the path velocity. |
| MC_GrpReadError | Reads the Group ErrorID in State ERRORSTOP. |
| MC_GrpReadStatus | Returns the status of an axes group. |
|
Copyright © 2015 Kollmorgen™ |
|