You are here: Technical References > Motion Library > Motion/Pipe Network > MLGearInit

FunctionMLGearInitPipe Network motion icon

Description

Initializes a Gear Pipe Block for use in a PLC"Programmable Logic Controller" A Programmable Logic Controller, PLC, or Programmable Controller is a digital computer used for automation of industrial processes, such as control of machinery on factory assembly lines. Used to synchronize the flow of inputs from (physical) sensors and events with the flow of outputs to actuators and events Program. FunctionA function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. block is automatically called if a Gear Block is added to the Pipe Network, with user-defined settings entered in the Pipe Blocks Properties screen.

The Pipe Block is assigned a Name, Ratio, Offset, and Slopes for changes in Ratio and Offset values. You can also choose between Modulo or Not modulo mode. Slopes set the limit at which step changes in Ratio and Offset are implemented.

The output of a Gear Block = Input value * Ratio + Offset

Arguments

Input

BlockID

Description

ID number of a created Pipe Block

 

Data type

DINT

 

Range

[-2147483648, 2147483648]

 

Unit

n/a

 

Default

GEAR

Ratio

Description

Ratio of new Gear Pipe Block. Values lower then 1.0 can be entered, but require a leading zero (for example 0.8 instead of .8)

 

Data type

LREAL

 

Range

—

 

Unit

n/a

 

Default

1.0

Offset

Description

Offset of new Gear Pipe Block. Values lower then 1.0 can be entered, but require a leading zero (for example 0.8 instead of .8)

 

Data type

LREAL

 

Range

—

 

Unit

n/a

 

Default

0.0

UseUserRatioSlope

Description

FALSE to use the maximum Slope, causing an instantaneous gear change within one cycle. TRUE to use user-defined RatioSlope

 

Data type

BOOL

 

Range

0, 1

 

Unit

n/a

 

Default

FALSE

RatioSlope

Description

User-defined limit at which step changes in Ratio are implemented. Values lower then 1.0 can be entered, but require a leading zero (for example 0.8 instead of .8)

 

Data type

LREAL

 

Range

—

 

Unit

1/sec

 

Default

0.0

UseUserOffsetSlope

Description

FALSE to use the maximum Slope, causing an instantaneous gear change within one cycle. TRUE to use user-defined OffsetSlope

 

Data type

BOOL

 

Range

0, 1

 

Unit

n/a

 

Default

FALSE

OffsetSlope

Description

User-defined limit at which step changes in Offset are implemented. Values lower then 1.0 can be entered, but require a leading zero (for example 0.8 instead of .8)

 

Data type

LREAL

 

Range

—

 

Unit

User unit/sec

 

Default

0.0

Modulo

Description

TRUE when mode is modulo. Modulo mode adapts the output values according to the ModuloPosition (modulo)

 

Data type

BOOL

 

Range

0, 1

 

Unit

n/a

 

Default

FALSE

Output

Default (.Q)

Description

Returns TRUE if the Gear Pipe Block is initialized

See more details here

 

Data type

BOOL

 

Unit

n/a

Return Type

BOOL

Related Functions

MLBlkCreate

MLGearWriteRatio

Example

Structured Text

//Initialize a Gear Pipe Block named GEAR1 with:
// Ratio = 1,Offset = 0, User Ratio Slope OFF, User Ratio
// Slope = 0, Offset Slope = 0, and no Modulo
GEAR1 := MLBlkCreate( 'GEAR1', 'GEAR' );
MLGearInit( GEAR1, 1.0, 0.0, false, 0.0, false, 0.0, false);

Ladder Diagram

MLGearInit: LD example

 

Function Block Diagram

MLGearInit: FBD example

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™