You are here: Technical References > Motion Library > Motion/Pipe Network > MLPhaInit

FunctionMLPhaInitPipe Network motion icon

Description

Initializes a phaser Pipe Block. Returns TRUE if the function succeeded.

This function block is automatically called by the FunctionA function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. PipeNetwork(MLPN_CREATE_OBJECTS) if a Phaser Block is added to the Pipe Network, with user-defined settings entered in the Pipe Blocks Properties screen.

The Phaser Pipe Block is assigned a Name, OUTPUT_PERIOD, PHASE, PHASE_SLOPE_TYPE, and STANDBY_VALUE.

Arguments

Input

BlockID

Description

ID Name of a Phaser function block in the Pipe Network

 

Data type

DINT

 

Range

[-2147483648, 2147483648]

 

Unit

n/a

 

Default

—

ModuloPosition

Description

Rollover Position of the Phaser block

 

Data type

LREAL

 

Range

—

 

Unit

User unit

 

Default

360.0

Phase

Description

Amount of Phase adjustment

 

Data type

LREAL

 

Range

—

 

Unit

n/a

 

Default

0.0

UseUserSlope

Description

Setting determines if Max Slope or user-defined slope is used

 

Data type

BOOL

 

Range

0, 1

 

Unit

n/a

 

Default

Max Slope

PhaseSlope

Description

User-defined slope for making the phase adjustment

 

Data type

LREAL

 

Range

—

 

Unit

User unit/sec

 

Default

0.0

StandbyValue

Description

This value is output from the Phaser Block, when the pipe is active, until the MLPhaWritePhase function is executed.

 

Data type

LREAL

 

Range

—

 

Unit

n/a

 

Default

0.0

Output

Default (.Q)

Description

Returns True if the function block is successfully executing

See more details here

 

Data type

BOOL

 

Unit

n/a

Related Functions

MLPhaReadPhase

MLPhaReadSlope

MLPhaInit

MLPhaWritePhase

Example

Structured Text

//Initialize  a Phaser  Pipe Block named “PhaseAdjust” to a Modulo of 720, phase offset value of 30, use the Max Slope
MLPhaInit( PipeNetwork.PhaseAdjust , 720, 30, false, 30 , 10 );

Ladder Diagram

MLPhaInit: LD example

Function Block Diagram

MLPhaInit: FBD example

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™