You are here: Technical References > Motion Library > Motion/Pipe Network > MLPhaReadActPhase

FunctionMLPhaReadActPhasePipe Network motion icon

Description

Get the actual phase value of a phaser block.

If a “PHASE_SLOPE_USER” (refer to MLPhaReadSlope and MLPhaWriteSlope) value is being used, the new phase (refer to MLPhaWritePhase) isn’t set immediately; the phase will be ramped with the slope value from the old phase value to the new phase value. MLPhaReadActPhase returns this ramping value.

MLPhaReadPhase returns the new value and this also when the phaser is still ramping. If using max slope means no ramping MLPhaReadActPhase and MLPhaReadPhase return always the same value.

Arguments

Input

EnableEnable signal for the drive, Hardware-Enable with 24V signal to X8, Software-Enable command by setup Software, fieldbus or permanently set. Both are required for enabling the drive. Description  
  Data type  
  Range  
  Unit  
  Default  
BlockID Description ID Name of a Phaser function block in the Pipe Network
  Data type DINT
  Range [-2147483648, 2147483648]
  Unit n/a
  Default —

Output

OK Description  
  Data type  
  Unit  
Phase Description  
  Data type LREAL
  Unit  

Related Functions

MLPhaReadPhase, MLPhaWritePhase, MLPhaReadSlope, MLPhaWriteSlope

Example

Structured Text

 

Ladder Diagram

 

 

Function Block Diagram

 

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™