You are here: Technical References > Motion Library > Motion Library - Common > MLProfileBuild

FunctionMLProfileBuildPLCopen motion iconPipe Network motion icon

Description

This Function BlockA function block groups an algorithm and a set of private data. It has inputs and outputs. allows the application to create a cam profile that may be executed by a cam block in PipeNetwork or PLCopenA vendor -and product- independent worldwide association active in Industrial Control and aiming at standardizing PLC file formats based on XML. This FunctionA function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. Block will take input as cam data (see Cam Profile Editor's Cam Table for information) and profile properties from application data memory and compile the input data to a form the controller can use to calculate cam positions. The input cam data and profile properties are similar to the cam data entered in the IDE"Integrated development environment" An integrated development environment is a type of computer software that assists computer programmers in developing software. IDEs normally consist of a source code editor, a compiler and/or interpreter, build-automation tools, and a debugger’s Cam Editor and the runtimeIn computer science, runtime (or run-time) describes the operation of a computer program, the duration of its execution, from beginning to termination (compare compile time). Within KAS, runtime also refers to the virtual machine that manage the program written in a computer language while it is running’s Cam Profile Properties dialog. MLProfileBuild internally perform two functions:

  1. Compile the cam data (like the cam editor performs in the IDE).
  2. Puts the compiled profile into the profile object so it can be used by other Profile Function Blocks (provides similar functionality to MLProfileInit).

MLProfileBuild will compile the cam profile data specified at the CamData input and write the resulting profile to the CAM Profile object specified at input ProfileID. The created profile can then be used as an input to PLCopen Cam Function Blocks (MC_CamTblSelect, MC_CamIn, MC_CamOut), or any Pipe network Cam Profile Function/Function Blocks. When the operation is complete, the Done output will go high. If an error is encountered, the Error output will go high and the ErrorID output will return a error code. If the Error can be attributed to a specific profile element in the CamData array, ErrorElem will attempt to indicate the element in error.

CamProps_Ref Structure

The cam properties structure (CamProps_Ref) will contain the following data members:

Parameter Type Description
InputScale LREAL The input amplitude or master axis multiplier applied to the CAM profile
OutputScale LREAL The output amplitude or slave axis multiplier applied to the CAM profile
InputOffset LREAL input offset or master axis shift applied to the CAM profile
OutputOffset LREAL The output offset or slave axis shift applied to the CAM profile

See Master/Input offset for more information about the parameters which transform the cam profile.

CamData_Ref Structure

The Cam_Data function block input will be an array of CamData_Ref structures. Each element of the structure will contain the following data members:

Parameter Type Description
MasterIn LREAL master position (in the unit range [0 - InputScale])
SlaveOut LREAL slave position (in the unit range [0 - OutputScale])
SegType UINT Defines the segment type for the segment following the master positions defined by MasterIn.
CAM_SEGMENT_TYPE_POINT = Point 5th order polynomial)
CAM_SEGMENT_TYPE_LINE = Line (constant velocity segment)
CAM_SEGMENT_TYPE_PARABOLIC = Parabolic (constant acceleration)
See Cam Profile Segment Overview for information on the segment types.
Vel LREAL Cam velocity at the master position specified by MasterIn. Units: (slave position user units) / (master position user units)
Accel LREAL

For CAM_SEGMENT_TYPE_POINT:

Accel represents the cam acceleration at the master position specified by MasterIn. Units: (slave position user units) / (master position user units)

For CAM_SEGMENT_TYPE_LINE and CAM_SEGMENT_TYPE_PARABOLIC:

Accel is ignored.

The type of the Nth cam segment is defined by the Nth Cam_Data element. Since the cam will be constructed with one les segment than the Cam_Data elements, the last element's SegType will not be used.

See Cam Profile Editor's Cam Table for more information.

Arguments

Input

Enable

Description Enable execution. Starts on rising edgeA rising edge is the transition of a digital signal from low to high. It is also called positive edge.
  Data Type BOOL
  Range  
  Unit  
  Default  

Cam_Props

Description Structures containing the cam profile properties
Data Type CamProps_ref
Range  
Unit  
Default  

Cam_Data

Description Array of structures containing the cam profile data
Data Type CamData_ref
Range N=3 to 2000 elements
Unit  
Default 3 elements minimum size

CamDataCount

Description Number of elements in the Cam_Data array to be used.
Data Type UINT
Range 3 - 2000
Unit elements
Default 3

ProfileID

Description ID number of a created CAM Profile
Data Type DINT
Range [-2147483648, 2147483648]
Unit n/a
Default --

Cyclic

Description False:  one time through the profile; True: repeating profile
Data Type BOOL
Range 0-1 (FALSE/TRUE)
Unit  
Default  

Options

Description Describes the combinations of segments that may be used to build a cam profile.
Data Type UINT
Range CAM_PROFILE_OPTION_DEFAULT: Allows the use of point and line segments.
CAM_PROFILE_OPTION_PARABOLIC: Allows the use of line and parabolic segments.

  • The DEFAULT and PARABOLIC options cannot be combined. A cam profile can only use point and line segments, or parabolic and line segments. Point and parabolic segments cannot both be used in the same profile.
Unit  
Default  

Output

Done

Description Indication of whether or not the profile was successfully compiled and built.
Data Type BOOL
Range 0-1 (FALSE/TRUE)
Unit  

Busy

Description Indication that the function block is executing. TRUE if executing. False if not executing.
Data Type BOOL
Range 0-1 (FALSE/TRUE)
Unit  

Err

Description Indication that the function did not execute correctly. ErrorID output will be valid and indicate the reason.
Data Type BOOL
Range 0-1 (FALSE/TRUE)
Unit  

ErrorID

Description Indication of the reason for the failure to execute properly. See Error Codes table.
Data Type INT
Range  
Unit  

ErrorElem

Description The array element number of the cam data where an error is detected
Data Type UINT
Range  
Unit  

Error Codes

ErrorID Description
100 Cam_Data array does not have CamDataCount elements. The Cam_Data array is not large enough to hold the specified number of elements.
101 Invalid master or slave scale. The scale cannot be less than zero.
102 Element master or slave position is outside the range defined by Cam_Props.
103 A segment type was specified that is not supported by the value of the Options argument.
104 Master position of an element is too close to the master position of a previous element. 0.0005 * InputScale (see "CamProps_Ref Structure") is the minimum distance allowed.. Each element is compared to all previous elements. If the master distance between any two elements in the list are too close, this error will be generated.
106 Invalid profile ID. This can occur if the profile ID:
  1. does not exist
  2. has not been created yet
  3. profile ID is not a profile
107 CamDataCount exceeds maximum array size of 2000.
108 Profile is currently in use.
109 Attempting to build a profile already containing elements. Profile needs to be released first using MLProfileRelease.
110 The controller is running low on memory and could not allocate memory to hold the cam table data.
111 CamDataCount is not large enough. The minimum allowed value is 3.
112 For CAM_PROFILE_OPTION_PARABOLIC:  Elements are not sorted in increasing order by master position. After the first elelment, each element must have its master position be greater than the master position of the previous element.
113 For CAM_SEGMENT_TYPE_PARABOLIC: The average velocity for the segment is outside of range defined by start and end element velocities.
The following diagram illustrates the valid range for the average velocity.
200 First element's MasterIn value not equal to zero.
201 Last element's MasterIn value does not equal value of X-amplitude.
202 Cannot modify the first element in the cam element table. SlaveOut value is outside the output range specified by Cam_Props.
203 Cannot modify the last element in the cam element table. SlaveOut value is outside the output range specified by Cam_Props.

Related Functions

MLCamInit

MLCamSwitch

MLProfileCreate

MLProfileInit

MLProfileRelease

MC_CamIn

MC_CamOut

MC_CamTblSelect

Example of How to Use MLProfileBuild

Prior to using MLProfileBuild you must first create a profile. This must be done prior to MLMotionStart.

// Allocate space for a profile that will be built later
profileID := MLProfileCreate('ProfileName');

Next you need to define your profile data. This is done by creating an array of CamData_Ref structures in the data dictionary and then entering each of your elements into that newly created structure. In this example ProfileData is the name of the CamData_Ref structure.

// Define the profile data
ProfileData[0].MasterIn := 0.0;
ProfileData[0].SlaveOut := 180.0;
ProfileData[0].SegType := CAM_SEGMENT_TYPE_POINT;
ProfileData[0].Velocity := 0.0;
ProfileData[0].Acceleration := 0.0;

ProfileData[1].MasterIn := 180.0;
ProfileData[1].SlaveOut := 324.0;
ProfileData[1].SegType := CAM_SEGMENT_TYPE_POINT;
ProfileData[1].Velocity := 0.5;
ProfileData[1].Acceleration := -0.025;

ProfileData[2].MasterIn := 360.0;
ProfileData[2].SlaveOut := 240.0;
ProfileData[2].SegType := CAM_SEGMENT_TYPE_POINT;
ProfileData[2].Velocity := 0.0;
ProfileData[2].Acceleration := 0.0;

Now you need to define your profile properties. This is done by creating a CamProps_Ref structure in the data dictionary and then entering each of the properties into the newly created structure. In this example ProfileProps is the name of the CamProps_Ref structure.

// Define the profile properties
ProfileProps.InputScale := 360.0;  // Must be Positive!
ProfileProps.OutputScale := 360.0; // Must be Positive!
ProfileProps.InputOffset := 0.0;
ProfileProps.OutputOffset := 0.0;

Next call the MLProfileBuild Function Block in the IEC"International Electrotechnical Commission" IEC is a not-for-profit, non-governmental international standards organization that prepares and publishes International Standards for all electrical, electronic and related technologies language of choice. As part of this call it is recommended that you validate the Done and Error output before proceeding.

// Build the profile
Inst_MLProfileBuild( TRUE, ProfileProps, ProfileData, 3, ProfileID, TRUE, CAM_PROFILE_OPTION_DEFAULT);

Finally, after verifying that MLProfileBuild is Done and there are no errors, you can proceed and use the newly generated profile. The next step depends on the motion engine in use.

// Switch Pipe Network Profile
MLPrfWriteIScale(profileID, ProfileProps.InputScale);
MLPrfWriteOScale(profileID, ProfileProps.OutputScale);
MLPrfWriteIOffset(profileID, ProfileProps.InputOffset);
MLPrfWriteOOffset(profileID, ProfileProps.OutputOffset);
MLCamSwitch(PipeNetwork.CAM, profileID);

Example of Building a Parabolic Cam Profile

In order to build a parabolic cam profile, your cam data elements must use CAM_SEGMENT_TYPE_PARABOLIC or CAM_SEGMENT_TYPE_LINE when defining the cam data array:

// Define the profile data
ProfileData[0].MasterIn     := 0.0;
ProfileData[0].SlaveOut     := 0.0;
ProfileData[0].SegType      := CAM_SEGMENT_TYPE_PARABOLIC;
ProfileData[0].Velocity     := 0.0;
ProfileData[0].Acceleration := 0.5;

ProfileData[1].MasterIn     := 50.0;
ProfileData[1].SlaveOut     := 150.0;
ProfileData[1].SegType      := CAM_SEGMENT_TYPE_LINE;
ProfileData[1].Velocity     := 5.0;
ProfileData[1].Acceleration := 0.0;		// Not used

ProfileData[2].MasterIn     := 55.0;
ProfileData[2].SlaveOut     := 175.0;
ProfileData[2].SegType      := CAM_SEGMENT_TYPE_PARABOLIC;
ProfileData[2].Velocity     := 5.0;
ProfileData[2].Acceleration := 0.0;		// No limit to the acceleration rate of the segment.

ProfileData[3].MasterIn     := 105.0;
ProfileData[3].SlaveOut     := 250.0;
ProfileData[3].SegType      := CAM_SEGMENT_TYPE_PARABOLIC;
ProfileData[3].Velocity     := 0.0;
ProfileData[3].Acceleration := 0.5;

ProfileData[4].MasterIn     := 225.0;
ProfileData[4].SlaveOut     := 125.0;
ProfileData[4].SegType      := CAM_SEGMENT_TYPE_PARABOLIC;
ProfileData[4].Velocity     := -10.0;
ProfileData[4].Acceleration := 0.5;

ProfileData[5].MasterIn     := 360.0;
ProfileData[5].SlaveOut     := 0.0;
ProfileData[5].SegType      := CAM_SEGMENT_TYPE_PARABOLIC;	// Not used
ProfileData[5].Velocity     := 0.0;
ProfileData[5].Acceleration := 0.0;		// Not used

When calling the MLProfileBuild function block, make sure CAM_PROFILE_OPTION_PARABOLIC is specified for the Option argument: in the IEC language of choice. As part of this call it is recommended that you validate the Done and Error output before proceeding.

// Build the profile
Inst_MLProfileBuild( TRUE, ProfileProps, ProfileData, 3, ProfileID, TRUE, CAM_PROFILE_OPTION_PARABOLIC);

Code Examples

Structured Text:

// Build the profile
Inst_MLProfileBuild( TRUE, ProfileProps, ProfileData, 3, ProfileID, TRUE, CAM_PROFILE_OPTION_DEFAULT);

Function Block Diagram:

Ladder Diagram:

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™