You are here: Tools > Cam Profile Editor > Cam Profile Segment Overview

Cam Profile Segment Overview

Point Segment Type

Supported by KAS IDE"Integrated development environment" An integrated development environment is a type of computer software that assists computer programmers in developing software. IDEs normally consist of a source code editor, a compiler and/or interpreter, build-automation tools, and a debugger Profile Editor, MLProfileBuild (default option)
Segment Curve Velocity Acceleration Jerk
Continuous velocity
Continuous acceleration
Interpolation method 5th order polynomial. f(x) = Ax5 + Bx4 + Cx3 + Dx2 + Ex + F
Advantages With only a few segments, this type can be used to define profiles with continuously changing accelerations. For example, sinusoidal profiles can be emulated with 6 to 12 point segments.
Disadvantages One must specify the velocity and acceleration at the endpoints for each segment. It is difficult to use the point segment type to define constant acceleration or constant velocity segments.

Line Segment Type

Supported by KAS IDE Profile Editor, MLProfileBuild
Segment Curve Velocity Acceleration Jerk
Continuous velocity
Continuous acceleration
Interpolation method Linear function. f(x) = Ax + B
Advantages This segment type easily defines constant-velocity segments. It can be used in very large numbers to define profiles of any size without having to specify the velocity or acceleration at the segment endpoints.
Disadvantages Profiles can result in discontinuous velocities.

Parabolic Segment Type

Supported by KAS IDE Profile Editor, MLProfileBuild (parabolic option)
Segment Curve Velocity Acceleration Jerk
Continuous velocity
Continuous acceleration
Interpolation method Linear function: f(x) = Ax + B
and a 2nd order polynomial: f(x) = Cx2 + Dx + E
Advantages This segment type is used to define constant acceleration portions of a profile. This minimizes the peak acceleration needed to move from one cam point to another. This can be useful when the motors cannot support the accelerations used by other segment types.
Disadvantages Acceleration is discontinuous which can lead to additional electrical stress on the drives and motors.

In the example shown, the blue line represents the linear (constant velocity) part of the segment, while the black lines represent the parabolic (constant acceleration) parts of the segment.

Spline Segment Type

Supported by KAS IDE Profile Import. The points are created by separate software and is imported into KAS IDE project.
Segment Curve Velocity Acceleration Jerk
Continuous velocity
Continuous acceleration
Interpolation method 3rd order polynomial. f(x) = Ax3 + Bx2 + Cx + D
Advantages With only a few segments, this segment type can be used to define profiles with continuously changing velocities. Only the positions of the master and slave need to be specified. This produces smoother profiles than using line segments.
Disadvantages Since only positions are specified, the user has less control over the velocities and accelerations that occur throughout the profile.

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™