You can connect to a PDMM, PCMM, or AKC from an external network using VPN or other tunneling protocol. To do so you must open the following ports which are used by KAS to connect to a controller.
| Port | Component/Protocol using the port |
|---|---|
| 80 | KAS IDE"Integrated development environment" An integrated development environment is a type of computer software that assists computer programmers in developing software. IDEs normally consist of a source code editor, a compiler and/or interpreter, build-automation tools, and a debugger: Controller Web Server; Download PLC application; Runtime front end communication. This is necessary for the connection to the runtime. |
| 502 | HMI and other Modbus devices to communicate with Modbus TCP. |
| 2222 | Ethernet/IP communication |
| 4002 | KAS IDE: Oscilloscope variable monitoring. |
| 4003 | KAS IDE: Communication with the PLC"Programmable Logic Controller" A Programmable Logic Controller, PLC, or Programmable Controller is a digital computer used for automation of industrial processes, such as control of machinery on factory assembly lines. Used to synchronize the flow of inputs from (physical) sensors and events with the flow of outputs to actuators and events Virtual Machine. This is necessary for the connection to the runtime. |
| 9900 | KAS IDE: Communication with the runtime engine; WorkBenchviews. This is necessary for the connection to the runtime. |
| 34962 | Profinet communication |
| 34964 | Profinet communication |
| 44848 | Ethernet/IP communication |
|
Copyright © 2015 Kollmorgen™ |
|