The EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs nodes provide several types of diagnostic information through various registers. The KAS controller uses these diagnostic registers to detect error conditions in the EtherCAT network. This can include:
| Physical Link status | Indicates if a hardware connection between two nodes is established. |
| Link Lost Counter | Indicates how many connection lost events have occurred between two nodes. Some EtherCAT devices will not detect the lost link event. |
| Rx Error Counter | This counter is incremented when the node detects any signal error detected by the hardware. |
| Rx Invalid Frame Counter | Invalid frame error is detected when the CRC"Cyclic redundancy check" A CRC is a type of function that takes as input a data stream of any length and produces as output a value of a certain fixed size. The term CRC is often used to denote either the function or the function's output. A CRC can be used as a checksum to detect accidental alteration of data during transmission or storage (Cyclic Redundancy Check) does not match the received frame CRC. |
| Forwarded Rx Error Counter | FrameIn networking dialect, a message is called a frame error detected by the previous node and forwarded to this node. |
| EtherCAT Processing Unit Error Counter | Counts errors in the EtherCAT frames such as frame length or a non-EtherCAT frame. Not all EtherCAT devices support this register. |
The node register of Link Lost Counter, Rx Error Counter, Rx Invalid Frame Counter, Forwarded Rx Error Counter, and EtherCAT Processing Unit Error Counter will have non-zero values when a cable disconnection or an EtherCAT frame corruption occurs, The following example indicates that a communication failure occurred between Node 0 and Node 1.
EtherCAT | WARNING | EtherCAT diagnostics: Node 0, port B (out), Rx Invalid Frame Counter Register is 255
EtherCAT | WARNING | EtherCAT diagnostics: Node 1, port A (in), Rx Invalid Frame Counter Register is 255
|
Copyright © 2015 Kollmorgen™ |
|