You are here: Annexes > List of Projects

List of Projects

The following projects provide real-life applications that illustrate how to use the functions:

Hole punch

Description

 

There are three axes as referenced on the picture:

  • Lower Rotary Axis (see call out )
  • Upper Rotary Axis
  • Linear Axis

This application is composed of two discs (one with pegs and the other with holes) that rotate (axes 1 and 2) independently and with different speed profiles. The motion is controlled to punch the two discs together (axis 3) when they match.

Each of the three axis is connected to an AKD drive.

Main Features

Initialize the motion

– MC_Power (in FFLD)

Make absolute and relative moves with the rotary axes

– MC_MoveAbsolute

– MC_MoveRelative

– MC_MoveSuperimp

– MC_MoveVelocity

Synchronize the axes

– MC_CamTblSelect

– MC_GearIn

– MC_Phasing

Manage the motion

– MC_ReadActPos (in FFLD)

– MC_ReadParam (in FFLD)

– MC_ReadStatus (in FFLD)

– MC_ReadActVel (in FFLD)

– ECATGetStatus (in FFLD)

Stop the motion

– MC_Halt

– MC_EStop (in FFLD)

– MC_ResetError (in FFLD)

– MC_ClearFaults (in FFLD)

 

Main

Common Functions (FFLD)

Homing Hole Punch

 

 

Hole Punch Project


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™