You are here: KAS IDE Reference > Configuring EtherCAT > ESI File Management

ESI File Management

ESI files which are referenced from a project's EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs devices are stored in the project.

ESI files will be replaced when: 

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™