You are here: KAS IDE Reference > Configuring EtherCAT > ESI Files tab

ESI Files

This tab lists the available ESI (EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs Slave Information) files and provides the ability to add and remove files.

ESI files are sorted by vendor and then the files provided by the vendor. Each file lists the device it supports including

ESI files are easily added to the list by clicking the Add button and navigating to where the file is saved. The Delete button will remove a file from the list but not your hard drive.

ESI files will be replaced when: 

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™