You are here: Getting Started > Creating a Project > Step 2 - Configure EtherCAT Motion Bus > Scan and Associate Network Devices

Scan and Associate Network Devices

To discover the physical EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs devices, follow these steps:

  1. In the Project Explorer, double-click the EtherCAT node to open the Devices tab. If there are no devices, the EtherCAT network topology has not yet been scanned and discovered.
  2. In the Devices tab, click the Scan Devices button.
  3. Press OK. The devices will appear in the Devices tab and in the Project Explorer. Their associated project devices are set to the defaults.

To change the device associations see Re-Scan and Change Device Associations.

To troubleshoot an error due to a missing ESI file, please see Unknown – Missing ESI File.

Concept Link IconSee Also

 

Unknown - Missing ESI File

Missing ESI File - MDP Device


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™