You are here: KAS IDE Reference > Create Programs > ST / IL Editor > Intellisense

Intellisense

The following features are available with Intellisense in ST"Structured text" A high-level language that is block structured and syntactically resembles Pascal and FBD"Function block diagram" A function block diagram describes a function between input variables and output variables. A function is described as a set of elementary blocks programs:

Conditional compiling coloring

Parts of conditional compiling code (declared with #ifdef pragmas) that are not validated are grayed

Commenting the CONDITION changes the active part of the program

Auto-indentation

Lines are automatically indented on the left when you enter structured ST statements

Autocompletion

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™