You are here: KAS IDE Reference > Create Programs > ST / IL Editor

Structured Text (ST) / Instruction List (IL) Editor

The ST"Structured text" A high-level language that is block structured and syntactically resembles Pascal / IL"Instruction list" This is a low-level language and resembles assembly editor is a powerful language-sensitive text editor dedicated to IEC"International Electrotechnical Commission" IEC is a not-for-profit, non-governmental international standards organization that prepares and publishes International Standards for all electrical, electronic and related technologies 61131-3 languages. The editor supports advanced graphic features such as drag-and-drop, syntax coloring and active tooltips for efficient input and test of programs in ST and IL.

Related sections:

Language selection
Syntax coloring
Autocompletion of words
Drag-and-drop
Active tooltips
Selecting function blocks
Inserting variable and FB instances symbols
Reading output of a FB instance
Bookmarks

Concept Link IconSee Also

 

ST / IL Language Selection

Syntax Coloring

Intellisense

Autocompletion

Drag-and-Drop Text

Read Output of a Function Block in ST


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™