| AKD | PDMM or PCMM | I/O Slice | Third-Party Devices |
|---|---|---|---|
| Double-click on the drive and select the I/O tab | Double-click Controller Onboard I/O | Double-click the I/O Slice in the Coupler entry. | Double-click the device and select the PDO Selection/Mapping tab. |
![]() | ![]() |


The Unmap command in the contextual menu (see figure in step 5 above) allows you to remove the link between the variable and the associated channel(s). In addition, deleting a variable from the dictionary which is mapped to the channel(s) also removes the link(s).
|
Copyright © 2015 Kollmorgen™ |
|