You are here: KAS IDE Reference > Map Input and Output to Variables > PLC Variable Selector

PLC Variable Selector

Create PLC Variable Button

This button allows the creation of a new variable to be mapped to the selected item(s).

Field Description
Scope Defines where the variable is created
Name See Name a variable
Type Defines the Type of the variable, and its Dimension if the variable is an array
Dimension The dimension of the variable (read-only). The dimension is set automatically based on the necessary size and the selected variable type.
Init Value See Initial Value of a Variable

See also Create Variables

Advanced Button

For integer variables with types stored on several bits, the Advanced button gives access to the Start bit definition. This allows you to link a set of channels to a specific range of bits within an integer variable.

For example, when you select three channels ranging from 1 to 3 and map them to a DINT variable (stored on 32 bits ranging from 0 to 31), the first channel can be linked to position ranging from 0 to 29.

The three channels are mapped to the last three bits ranging from 29 to 31.

Concept Link IconSee Also

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™