You are here: Understanding KAS > IEC 61131-3 > Data Types > Arrays

Arrays

You can declare arrays for internal variables by specifying dimension(s).

To declare an array, enter the number of elements in the Dim. column of the Dictionary (see procedure here).

Declare an Array for an Internal Variable

For a multi-dimensional array (note that arrays have at most three dimensions), enter the number of elements for each dimension separated by commas (for example 2,10,4 is a 3 dimensional array, the first dimension has 2 elements, the second dimension has 10 elements, and the third dimension has 4 elements).

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™