You are here: Describing KAS Graphical User Interface > Windows and Panels Overview > Dictionary > Variables Tab
List of variables Track Selection List of structures HMI

Variables tab

The Variables tab is used to show all the variables defined within the project. All the variable details are displayed in order to show the variable types, dimensions, attributes, etc.

Dictionary Toolbox

Figure 3-5: Dictionary Toolbox

The list of variables is split into two parts:

Concept Link IconSee Also

 

Variables

Structures

Variable Editor

Variable Table List

Sort Variables

Define Structures

Name a Variable

Rename Variables

Initial Value

Tag and Description

Editing Variables as Text Using IEC 61131-3 Syntax


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™