The web server displays an error message if an EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs Device backup or restore fails. The message describes the cause of the failure and a possible remedy. Please be sure to note any error message(s), as they will be helpful with remedying the problem.
Described below are some common error messages and remedies. The message box format may appear differently depending on the web browser, but the message content is the same.
Before restoring AKD(s), the backup file must be valid. To correct a bad backup file on a controller, import a known good backup file from another source (local hard drive, network drive, USB"Universal Serial Bus" USB is a serial bus standard to interface devices flash stick, etc.). If you do not have a valid backup file, then you will need to manually configure the replacement AKDs by downloading firmware and modifying the drive’s parameters using the AKD views in the IDE.
The error message will describe at which step the restore failed. For example, failing to restore parameters:
|
Copyright © 2015 Kollmorgen™ |
|