You are here: Using the PDMM or PCMM Controller > Working with the Hardware > About Errors and Alarms

About Errors and Alarms

The PDMM or PCMM controller will continuously display any error or alarm codes after booting, and not in recovery mode.

Only one error or alarm code will be displayed at a time. Errors have a priority over Alarms and the code with the highest priority will be displayed until it is cleared.

Error code example Alarm code example

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™