You are here: Using the PDMM or PCMM Controller > Working with the Hardware > Display the IP Address of a PDMM or PCMM

Display the IP Address of a PDMM or PCMM

The IP Address assigned to the controller can be shown on the 7-segment display. The IP may be displayed at boot and can be accessed from the PDMM or PCMM B3 Button Menu. Note that there is a 5 second delay before this function may be used again.

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™