You are here: Using the PDMM or PCMM Controller > Working with the Hardware > SD Card Support

SD Card Support

The PDMM and PCMM controllers support using an SD card for backup and restore functionality. This lets you manage the configuration, application and operation data. The controller has a SD card slot and push buttons (B2 and B3) which activate file transfers to and from a SD card.

Using the SD card provides an easy way to

Supported SD Card Formats

Format File System Capacity
SD (SDSC) FAT16‡ or FAT32 2GB
SDHC FAT32‡ 4-32GB

‡ The default file system for the format.

See SD Card Access for information on mounting/checking/unmounting SD cards using FBs.

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™