KAS provides start up templates to help you get started (see how to use the project setup wizard here). There are separate templates for the Pipe Network motion engine and for the PLCopenA vendor -and product- independent worldwide association active in Industrial Control and aiming at standardizing PLC file formats based on XML motion engine:
These templates come complete with software to:
The templates contain variables which support these operations.
Additionally, the templates contain a Control Panel for ease of running motion.
You may need to modify the templates to run on your specific hardware.
Pipe Network with SFC (SFC, ST, FFLD and FBD)
PLCopen with SFC (SFC and FFLD)
Coordinated Motion 2-Axis Template
|
Copyright © 2015 Kollmorgen™ |
|