You are here: Troubleshooting > EtherCAT Coupler Error Handling and Diagnosis > LEDs for EtherCAT State Machine/PLC Diagnosis

LEDs for EtherCAT State Machine/PLC Diagnosis

LEDs   Display Status Description
Run Green Off Init State of the EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs State MachineThe complete assembly of all connected parts or devices, of which at least one is movable: INIT = Initialization
Blinking Pre-operational State of the EtherCAT State Machine: PREOP = Pre-Operational
Single Flash Safe operational State of the EtherCAT State Machine: SAFEOP = Safe-Operational
On Operational State of the EtherCAT State Machine: OP = Operational
Flashes Bootstrap State of the EtherCAT State Machine: BOOT = Bootstrap (Update of the coupler firmware)
Error Red Off — No errors
Blinking Err-Operational No Communication PLC"Programmable Logic Controller" A Programmable Logic Controller, PLC, or Programmable Controller is a digital computer used for automation of industrial processes, such as control of machinery on factory assembly lines. Used to synchronize the flow of inputs from (physical) sensors and events with the flow of outputs to actuators and events error / Lost frames

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™