You are here: Understanding KAS > IEC 61131-3 > Variables > Retain Variables

Retain Variables

What is a retain variable?

A retain variable is a PLC"Programmable Logic Controller" A Programmable Logic Controller, PLC, or Programmable Controller is a digital computer used for automation of industrial processes, such as control of machinery on factory assembly lines. Used to synchronize the flow of inputs from (physical) sensors and events with the flow of outputs to actuators and events variable which:

Such a variable is used to store application specific data, like for instance to count a cutting-edge cycle in order to stop for its blade replacement after a specific number of iterations.

Two parameters are checked to identify if the declaration changed:

For the KAS RuntimeIn computer science, runtime (or run-time) describes the operation of a computer program, the duration of its execution, from beginning to termination (compare compile time). Within KAS, runtime also refers to the virtual machine that manage the program written in a computer language while it is running Simulator, the retained variables are saved in a file in your project repository.

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™