You are here: KAS Component Manuals > Controllers > NVRAM

NVRAM

KAS uses the NVRAM"Non-volatile random access memory" NVRAM is the general name used to describe any type of random access memory which does not lose its information when power is turned off. This is in contrast to the most common forms of random access memory today, which both require continual power in order to maintain their data. NVRAM is a subgroup of the more general class of non-volatile memory types, the difference being that NVRAM devices offer random access, like hard disks. The best-known form of NVRAM memory today is flash memory (non-volatile memory) to save Retain Variables.

Hardware Type NVRAM Size Allocation
Old generation PAC"Programmable Automation Controller" PAC is a compact controller that combines the features and capabilities of a PC-based control system with that of a typical programmable logic controller (PLC). A PAC thus provides not only the reliability of a PLC, but also the task flexibility and computing power of a PC. Additionally, because they function and communicate over popular network interface protocols, PACs are able to transfer data from the machines they control to other machines and components in a networked control system 32 Kbytes
New generation PAC 128 Kbytes
Simulator 128 Kbytes
PDMM or PCMM 32 Kbytes

Table 12-3: NVRAM Size Depending on Hardware

If the size is big enough, KAS updates the non-volatile memory to store the retain variables values. This operation is performed in the background every 20 seconds. The frequency increases to every 2 seconds when the application is running, and when you shutdown the application.

How can I check the NVRAM space is enough to store my retain variables?

To calculate the NVRAM space, you have to add the size of each retained variable according to:

Do not forget to add the 144 bytes as stated in the Warning above.

In the following example, the total size is: 3684 bits (which is less than 0.5 Kbytes)

Variable Size / element Element no. Total Size / variable
bLedStatus 1 bit 4 4
MasterAbsPos 64 bits 1 64
MyString 800 bits (100 bytes) 3 2400
TravelSpeed 64 bits 1 64
Internal data 1152 bits (144 bytes) na 1152

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™