Open topic with navigation
A full circle may be performed using the following procedure.
MC_CIRC_MODE_CENTER
MC_CIRC_MODE_BORDER cannot be used because it is limited to angles <360°.
Stay Connected with Kollmorgen
Copyright © 2015 Kollmorgen™