You are here: Advanced Topics > Coordinated Motion > How-To: Coordinated Motion > Performing a Linear Move

Performing a Linear Move

Linear moves can be programmed using absolute or relative positions using the following function blocks:

Prior to performing any coordinated moves, some setup is needed (see "Create a Linear or Circular Coordinated Motion Application"). Once these steps have been performed, a linear move can be performed.

In the following examples, two linear moves will be performed. The first move is an absolute linear move that goes from (0, 0) to (100, 200). The second move is a relative linear move that goes a distance of (-75, 50) from the end of the first move.The BufferMode input is set to 'Buffered', meaning this move will wait for the first move to complete before it begins executing.

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™