You are here: Advanced Topics > Coordinated Motion > How-To: Coordinated Motion > Line to Line Transitions

Line to Line Transitions

When both moves are linear the current and next moves are shortened using this transition mode. The amount is specified by the corner distance. A circular arc connects the two moves (except as noted below), allowing for a smooth transition (see n-Degree Transition below). The circular arc that connects the two moves derives its velocity from the transition parameter and the acceleration and deceleration values are derived from the next move.

Motion Path - Line to Line Key Motion Velocity Profile

Blue: Incoming, outgoing linear motion

Red: Transition arc

  1. Original endpoint of 1st move
  2. Corner distance

Figure 11-2: n-Degree Transition

Blue: Incoming linear motion

Red: Outgoing linear motion

  1. Original endpoint of 1st move
  2. Corner distance

Figure 11-3: 180-Degree Transition: New move is in the opposite direction as old move. The sudden change in the direction of motion may result in large jerks to the axes

Blue: Incoming, outgoing linear motion

Red: Transition line segment

  1. Original endpoint of 1st move
  2. Corner distance

Figure 11-4: 0-Degree Transition: New move continues in same direction as old move — continuous behavior

Blue: Incoming, outgoing linear motion

Red: Zero distance transition move

  1. Original endpoint of 1st move

Figure 11-5: 0-Distance Transition: Motion passes the first move's endpoint . There is no transition arc. A sudden change in the direction of motion may result in large jerks to the axes.

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™