You are here: Technical References > Remote Access to PLC Variables > Introduction to Read and Write PLC Variables Via HTTP Interface

Introduction to Read and Write PLC Variables Via HTTP Interface

The PLC"Programmable Logic Controller" A Programmable Logic Controller, PLC, or Programmable Controller is a digital computer used for automation of industrial processes, such as control of machinery on factory assembly lines. Used to synchronize the flow of inputs from (physical) sensors and events with the flow of outputs to actuators and events variable interface provides following features and advantages:

There are two interfaces:

The URL is same for both interfaces: (controller URL)/kas/plcvariables

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™