You are here: Technical References > Remote Access to PLC Variables > Using the HTTP Interface with C++

Using the HTTP Interface with C++

Third party libraries are needed to use the HTTP interface with C++. The libraries are used for parsing and generating JSON objects and as a client for sending HTTP requests. We recommend the following two libraries:

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™