You are here: Technical References > Application Modules > Circular and Linear Interpolation - PLC

Circular and Linear Interpolation w/ PLCopen Motion Engine

Introduction

This application example details sample code for a 3 axis system:

PLC Program Code

The application code provided with this application module is contained in four programs (that can be exported then imported into a project):

Program Name FunctionA function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. Language
Main Initialize the axis, the axis group, and motion Sequential Function Chart(SFC) with Structured Text (ST)
Jogging Jog the axes Structured Text (ST)
CircleDiamondSquare Perform homing and the circle, diamond, square motion FFLD (Free Form Ladder Diagram)
Common Common application functionality: Error ResetNew start of the microprocessor, Power Axis On/Off, EnableEnable signal for the drive, Hardware-Enable with 24V signal to X8, Software-Enable command by setup Software, fieldbus or permanently set. Both are required for enabling the drive. Group Motion, Read Axis Status, Read Axis Positions, Read Axis Group Positions FFLD (Free Form Ladder Diagram)

The key function blocks and Kollmorgen UDFBs used in the application:

Name Function Program
MC_InitAxesGrp Home the axis Main
MC_AddAxisToGrp Set a motor/load position after homing Main
IMC_GrpEnable Enable the group motion Common
MC_GrpReadActPos Read group position Common
MC_ReadActPos Read individual axis positions Common
MC_ReadStatus Read axis status Common
MC_Power Power an axis Common
MC_MoveRelative Make a relative move CircleDiamonSquare
MC_SetPosition Establish axis position after homing CircleDiamonSquare
MC_SetHomePosition Establish home position for the axis group CircleDiamonSquare
MC_MoveLinAbs Move 2 axis (x, y) linear interpolation move CircleDiamonSquare
MC_MoveCircAbs Move 2 axis (x, y) circular interpolation move CircleDiamonSquare

Main Program

The main program consists of 2 steps: Setup and IDLE:

In the Setup step:

Jogging Program

The Jogging Program allows motor jogging in either direction. The following is the code for the X axis. The Y and Z axis are similar:

CircleDiamonSquare Program

The CircleDiamondSquare program performs 2 axis coordinated motion. Key parts of the program are as follows:

  1. Network 2: Define default CM (coordinated motion) absolute positions, CM transition and CM move parameters. This is a large section that defines the starting parameters in the application. This network is executed once on program startup. Values can be change using the control panel ( CP_CircleDiamondSquare).
  2. 2. Network 3: DisableRemoval of the ENABLE signal. Disables power stage. limit switches before homing:

  3. Network 4: Reset both single axis and CM axes command and actual positions to zero before any homing sequence. This is necessary so the summed super imposed axis positions are 0 and will not affect single axis motion.

  4. Network 5: Home axes to limit switches after operator input. If the axis is on the limit switch back off first. Move to the axis 0 and set the position to 0.

  5. Network 6: End limits and home switches are common for each axis, therefore the re-enable of end limits after the axis home sequence is completed is performed:

  6. Network 7: Move X and Y axis to starting point. Move Z to starting point

  7. Network 8: Lower knife to contact point

  8. Networks 10 to 13: Make Square CM move. The starting position is the center or half way distance point of the top segment. This is required so the final corner of the square will transition with a radius. If the starting point was at the corner then the last segment would not be a radius. This starting position is also the ending point for the square. Restart the segment move if it has been halted while in motion.



  9. Network 15: Make circle move. The default circle center XY positions are based on the square center point.

  10. Network 19: Make diamond move

Common Program

The Common Program performs standard functions used in many applications.

  1. This code powers up the axis and the axis group:



  2. The following outputs the present motion status of each axis (only X axis shown):

  3. The following outputs actual positions of each axis and the group (only X axis shown):



Key Drive I/O

For each of the X, Y, and Z axes an input on the drive (on connector X7) was mapped for the axis homing functionality. The following shows the X axis mapping:

Control Panel

A Control Panel has been created to run the program:

Motion

These bottons determine what motion is run. To jog the motors, select Jog in the Jog/Run bottom. To make a circle, diamond, square shape select Run and then the switch for the appropaite figure type or select the run all button to run all 3 figures.

Setup Parameters

These parameters setup the circle, diamond, or square motions.

Axis Position

Axis and Group Positions are both shown.

Jogging

These controls are for the jogging motion.

Top Buttons

  1. To make a circle, diamond, and/or square motion:
  2. Code has been added to the program to stop and restart along the path during the square motion move:

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™