You are here: Technical References > Application Modules

Application Modules

This section contains Application Modules, which are examples of how KAS was used to create custom controls for machines. Most of the application modules have been created using both PLCopenA vendor -and product- independent worldwide association active in Industrial Control and aiming at standardizing PLC file formats based on XML and PipeNetwork motion engines.

Name PLCopen PipeNetwork Description
Rotary Knife Yes Yes Sample code for a 2-axis feed and cut system
Index Stop Yes Yes Sample code for a 3-axis cut-to-length system
Flying Knife Yes   Sample code for a 4-axis feed and cut system
Form Fill & Seal Yes Yes Sample code for a 5-axis form, fill and seal system
Unwind-Rewind   Yes An entire project for a 4-axis unwind/rewind web system with a registration operation.

 

Circular and Linear Interpolation - PLC

Flying Knife - PLC

Form Fill Seal - PLC

Form Fill Seal - PN

Index-Stop - PLC

Index-Stop - PN

Rotary Knife - PLC

Rotary Knife - PN

Unwind-Rewind

Integrating Non-Standard I/O Devices Into a KAS EtherCAT Network with an AKC Controller


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™