You are here: Technical References > Application Modules > Index-Stop - PLC

Cut to Length (Index – Stop) PLC Open

Introduction

This application module details a 3 axis section of machine containing an unwind axis with dancer control, registration mark control axis making adjustments based on product registration marks, and a cutting knife axis using the PLCopenA vendor -and product- independent worldwide association active in Industrial Control and aiming at standardizing PLC file formats based on XML motion engine. The unwind axis maintains a desired tension on the product as the registration mark control axis; using registration marks on the product; positions the product. When in position the cutting knife will cut the product to the desired length.

  1. Motor drives from this point
  2. Unwinding
  3. Registration Mark Reader
  4. Registration Mark Control
  5. Cutting Knife
  6. Dancer Pot.
  7. Dancer

Unwind Axis

The unwind axis is geared to the virtual master axis. As the product is being unwound from the parent roll a dancer roll is monitoring the desired tension. If the tension is outside the desired adjustable dead band the gear ratio between the virtual master axis and unwind is adjusted to maintain the desired tension. The tension (Regulation TnIntegral component of a control loop), gain to control the tension (Regulation KpProportional gain of a control loop), minimum and maximum dead band (Deadband Min & Deadband Max) is entered on the control panel.

Figure 11-224: Unwind Base Profile

Registration Mark Control Axis

The registration mark control axis monitors the registration marks on the product and adjusts the product based on the registration mark parameters, Open Window, Close Window, and Reference Position entered on the operator panel. If the registration mark is detected between the Open Window and Close Window the registration mark is considered a good mark and the Reference Position value will be used to calculate the necessary adjustment. If the registration mark is detected outside the Open Window and Close Window values then the registration mark is ignored. Adjustments are not made during the cutting process to avoid destroying product.

Cutting Knife Axis

The cutting knife axis is geared to the master virtual axis based on a profile (CutKnife). The profile will start at the starting position of the virtual axis.

Figure 11-225: Cutting Knife Base Profile

PLC Program Code

Name How Used

MC_GearIn

Gears one axis to another

MC_CamIn

Gears one axis to another using a cam profile

MC_TouchProbe

Arms the fast inputThe inputs are taken into account at each cycle depending on the system periodicity (for example each millisecond). Under certain circumstances this can be insufficient when more accuracy is needed, or if a quick response is required from the system. To fill the gap, a drive may have some Fast Input connections (generally one or two). When an event happens that triggers a Fast Input (e.g. when a sensor sends a rising edge), the detection of a signal occurs faster (which can be 1000 times more accurate than the system periodicity). Then the timestamp associated with this input can be provided to the IPC to take corrective action and returns the latched position when the fast input occurs

MC_MoveVelocity

Moves a single axis at a specified velocity

MC_MoveSuperimp

Relative single axis move superimposed on an active move

FIFO

Manages first in/first out list

Table 11-56: Key Function Blocks and Kollmorgen UDFBs used in the Index-Stop application module

The main section of the PLC"Programmable Logic Controller" A Programmable Logic Controller, PLC, or Programmable Controller is a digital computer used for automation of industrial processes, such as control of machinery on factory assembly lines. Used to synchronize the flow of inputs from (physical) sensors and events with the flow of outputs to actuators and events code contains several If/Then statements. The program sets up gearing and cam profiles for the slave axis to a virtual master. The virtual master controls the machine speed. The slave axes are manipulated by either changing the operator panel inputs or profiles. The program is monitoring registration marks on the product and making correction to the product position based on the entries at the operator panel.

(* The following section of code gears the Unwind axis to the Virtualmaster2 axis and synchronizes the Virtualmaster2, RegAdjust, and Cutknife axes with the respective profiles ProfileIDUnwind and ProfileIDCutKnife. *)

CASE StepCounter OF

0:

Inst_MC_GearIn( TRUE, VirtualMaster2, Unwind, 1, 1, 10000, 10000, 0, 0 );

Inst_MC_CamIn( TRUE, VirtualMaster, VirtualMaster2, 0, 0, 360, 360, 0, ProfileIDUnwind, 0 );

Inst_MC_CamIn1( TRUE, VirtualMaster, RegAdjust, 0, 0, 360, 360, 0, ProfileIDUnwind, 0 );

Inst_MC_CamIn2( TRUE, VirtualMaster, CutKnife, 0, 0, 360, 360, 0, ProfileIDCutKnife, 0 );

 

(* The following section of code checks that the unwind axis is geared to the Virtualmaster2 axis and that the Virtualmaster2, RegAdjust, and Cutknife axes are synchronized with the respective profiles ProfileIDUnwind and ProfileIDCutKnife. If the axes are geared and synchronized and the machine start button is selected the master axis will be run at the desired velocity. *)

IF Inst_MC_GearIn.InGear AND Inst_MC_CamIn.InSync AND Inst_MC_CamIn1.InSync AND Inst_MC_CamIn2.InSync THEN

   StepCounter := 1;

END_IF;

 

1:

IF MachineStart THEN

IF MasterVelocity <> OldMasterVelocity THEN

      Inst_MC_MoveVelocity2( FALSE, VirtualMaster, MasterVelocity, 10000, 10000, 0, 0, 0 );

      Inst_MC_MoveVelocity2( TRUE, VirtualMaster, MasterVelocity, 10000, 10000, 0, 0, 0 );

      OldMasterVelocity := MasterVelocity;

END_IF;

ELSE

   OldMasterVelocity := 0;

END_IF;

 

(*********

Unwind Axis with Dancer Control

Monitor Dancer and change Gear Ratio between VirtualMaster and Unwind Axis to maintain desired tension

May also want to change gear ratio as the radius of feed material decreases due to web being used

Dancer range 0-10V, 5V mid, adjustable deadband, > deadband increase speed, < deadband decrease speed

*********)

IF MachineStart THEN

   Inst_DancerUnwindGear( TRUE, DancerAnalogSignal, Kp, Tn, DeadBandMin, DeadBandMax, CycleTime );

IF Inst_DancerUnwindGear.obOutsideDeadband THEN

      Inst_MC_GearIn( FALSE, VirtualMaster2, Unwind, any_to_dint((Inst_DancerUnwindGear.oUnwindGearRatio + 1)*10000000), 10000000, 10000, 10000, 0, 0 );

      Inst_MC_GearIn( TRUE, VirtualMaster2, Unwind, any_to_dint((Inst_DancerUnwindGear.oUnwindGearRatio + 1)*10000000), 10000000, 10000, 10000, 0, 0 );

END_IF;

END_IF;

 

//Registration Mark Control Axis

//Monitor registration marks and make adjustments to RegAdjust Axis

Inst_MC_TouchProbe( TRUE, RegAdjust, TriggerRef, FALSE, 0, 0 );

IF Inst_MC_TouchProbe.Done THEN

   RegistrationMarkPos := Inst_MC_TouchProbe.RecordedPosition;

   Inst_MC_TouchProbe( FALSE, RegAdjust, TriggerRef, FALSE, 0, 0 );

   Inst_MC_TouchProbe( TRUE, RegAdjust, TriggerRef, FALSE, 0, 0 );//Rearm for next registration mark

 

IF RegistrationMarkPos > OpenWindowPos AND RegistrationMarkPos < CloseWindowPos THEN //Check if mark was within good window

IF RegistrationMarkPos < ReferencePos THEN //Check if phase forward or backward is required

         NewAdjustment := ReferencePos-RegistrationMarkPos;

ELSE

         NewAdjustment := ReferencePos-RegistrationMarkPos;

END_IF;

 

      Inst_FIFO( FALSE, FALSE, FALSE, NewAdjustment, Adjustment, AdjustmentArray );

      Inst_FIFO( TRUE, FALSE, FALSE, NewAdjustment, Adjustment, AdjustmentArray );

IF Inst_FIFO.Count = 4 THEN

         Inst_FIFO( FALSE, FALSE, FALSE, NewAdjustment, Adjustment, AdjustmentArray );

         Inst_FIFO( FALSE, TRUE, FALSE, NewAdjustment, Adjustment, AdjustmentArray );

         NewMarkHit := TRUE;

END_IF;  

END_IF;

END_IF;

 

IF NewMarkHit AND ActPosVirtualMaster > 0 AND ActPosVirtualMaster < 45 THEN //Do not make adjustment during sealing process

   Inst_MC_MoveSuperimp( FALSE, RegAdjust, Adjustment, MasterVelocity*3, 10000, 10000, 0, 0 );

   Inst_MC_MoveSuperimp( TRUE, RegAdjust, Adjustment, MasterVelocity*3, 10000, 10000, 0, 0 );

   NewMarkHit := FALSE;

END_IF;

 

//CutKnife

 

END_CASE;

Operator Panel

The Kollmorgen Automation Suite (KAS) program for this application module has an internal operator panel. The operator panel is used to set the desired values for each product and to start and stop the machine. The specific entries are described in the axis sections above. Below is a screen print of the operator panel.

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™