4 axes with SFC"Sequential function chart" It can be used to program processes that can be split into steps. The main components of SFC are: - Steps with associated actions - Transitions with associated logic conditions - Directed links between steps and transitions/ST"Structured text" A high-level language that is block structured and syntactically resembles Pascal and Pipe Network Motion Engine
This document details a KAS 4 axis unwind/rewind web system with a registration operation. The 4 axis are as follows:
|
|
The machine can be run bi-directionally with the left roller as the unwind axis and right roller as the rewind axis or left roller as the rewind axis and right roller as the unwind axis. All four axes are tied to a virtual master using the KAS pipe network.
The web of material contains holes in it. The rotary die cutter axis is dynamically controlled to be in sync with the holes in the web.
|
|
The machine is run through a Kollmorgen AKI human machine interface:
There are multiple screens in the Kollmorgen AKI performing the following functions:
|
Copyright © 2015 Kollmorgen™ |
|