You are here: Technical References > Application Modules > Unwind-Rewind > Setup

Setup

User Units

Below is a summary of the user units used in the application. The virtual master, left winder and right winder have base units of degrees/sec. The draw roller and die cutter have base units of mm/sec. For the draw roller and die cutter the User Units (UU) per turn are calculated incorporating the diameters of the drive rollers. Note: DU = DriveControl device for regulating the speed, torque and position of a motor Units

Axis Gear Ratio DU per rev UU per turn Base Units UU per (motor) rev Axis Rollover

1 Left Winder

1

1048576

360 deg

deg/sec

DEF_A1_UUperTurn/DEF_A1_GearRatio = 360

360

2 Draw Roller

10

1048576

202.24mm

mm/sec

DEF_A2_UUperTurn/DEF_A2_GearRatio = 202.24/10 = 20.2

150

3 Die Cutter

1

1048576

300 mm

mm/sec

DEF_A3_UUperTurn/DEF_A3_GearRatio = 300/1 = 300

300

4 Right Winder

1

1048576

360 deg

deg/sec

DEF_A4_UUperTurn/DEF_A4_GearRatio = 360/1 = 360

360

Virtual Master

---

---

---

deg/sec

360

360

Defines

Purpose

In the project tree the Defines section contains value for project parameters to configure the project for a particular machine mechanics and desired machine performance. With Defines, the KAS application program can be tailored for a variety of machine types.

Defines can be used as compiler directives and set up the application for individual machine needs including for the following:

Status Mask

Status mask are used to setup the bit definitions of the Axis and Machine Status Words: A1_StatusWord, A2_StatusWord, and M1_StatusWord. Example: The bit masks for A1_StatusWord are:

Initial parameters in Pipe Network Blocks

These parameters are used to initialize the motion parameters in the pipe network block. Example: several of the following parameters are used to define the AX1_A1_Axis Pipe network block:

Machine States and Timers

Defines are used to define Machine States and Timer values

Load and Save Drive Parameters

Defines are used to help setup an array to  read and write AKD drive parameters into a PAC"Programmable Automation Controller" PAC is a compact controller that combines the features and capabilities of a PC-based control system with that of a typical programmable logic controller (PLC). A PAC thus provides not only the reliability of a PLC, but also the task flexibility and computing power of a PC. Additionally, because they function and communicate over popular network interface protocols, PACs are able to transfer data from the machines they control to other machines and components in a networked control system based file:

See Appendix for a full listing of defines

Ethercat Setup

Scanning

The system’s Ethercat network can be configured into the project by using the ‘Scan Devices’ feature once the controller has been connected to the items (drives and remote I/O) on the network.

Drive Setup

The commissioning of each drive can be accomplished by opening the AKD item. Once this is open each drive can be configured for line voltage, the motor and load including tuning, system limitations and the parameters. The available screens embedded in the KAS IDE"Integrated development environment" An integrated development environment is a type of computer software that assists computer programmers in developing software. IDEs normally consist of a source code editor, a compiler and/or interpreter, build-automation tools, and a debugger are similar, although not all the same, as the AKD GUI"Graphical User Interface" A GUI is a type of user interface which allows people to interact with a computer and computer-controlled devices View screens.

IO Setup

IO points can be set up in the project using the KAS IO support screens in the Ethercat section of the Project file

The value of the IO is displayed in the following Kollmorgen AKI screen:

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™