You are here: Tools > AKD into KAS > Workbench Reference > AIN.OFFSET

AIN.OFFSET

General Information

Type

NV Parameter

Description

Sets the analog input offset.

Units

V

Range

–10 to +10 V

Default Value

0 V

Data Type

Float

See Also

AIN Parameters on pg. 1, on pg. 1

Start Version

M_01-00-00-000

Variants Supported

FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design

Index/Subindex

Object Start Version

EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

5003h/0

M_01-00-00-000

Description

AIN.OFFSET sets the analog offset, which is added to the analog input command to the drive.  This value compensates for the analog input signal (AIN.VALUE on pg. 1) offset or drift.

Related Topics

Analog Input on pg. 1

on pg. 1

Block Diagram for Position/Velocity Loop on pg. 1

 

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™