You are here: Tools > AKD into KAS > Workbench Reference > AIN.VALUE

AIN.VALUE

General Information

Type

R/O Parameter

Description

Reads the value of the analog input signal.

Units

V

Range

-12.5 to +12.5 V

Default Value

N/A

Data Type

Float

Start Version

M_01-00-00-000

Variants Supported

FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design

Index/Subindex

Object Start Version

EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

3470h on pg. 1/4

3509h/0

M_01-00-00-000

Description

AIN.VALUE reads the analog input value after the value is filtered (as shown in the Analog Input Block Diagram).

Related Topics

Analog Input on pg. 1

on pg. 1

AIN.OFFSET on pg. 1

Block Diagram for Position/Velocity Loop on pg. 1

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™