You are here: Tools > AKD into KAS > Workbench Reference > AOUT.DEBUGSCALE

AOUT.DEBUGSCALE

General Information

Type

NV Parameter

Description

Sets the scale to be used for debug.

Units

N/A

Range

0.001 to 9,223,372,036,854,775.000

Default Value

1

Data Type

Float

Start Version

M_01-01-01-000

Description

AOUT.DEBUGSCALE sets the scale to be used for debug when AOUT.MODE on pg. 1 = 9 (debug mode).

Related Topics

Analog Output on pg. 1

AOUT.MODE on pg. 1

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™