You are here: Tools > AKD into KAS > Workbench Reference > BODE.FREQ

BODE.FREQ

General Information

Type

R/W Parameter

Description

Sets the frequency of the sine excitation source.

Units

Hz

Range

0 to 8,000 Hz

Default Value

0 Hz

Data Type

Float

Start Version

M_01-00-00-000

Description

BODE.FREQ sets the frequency of the sine excitation source in Hz. The sine excitation source is used to take frequency response measurements of a system.

Example

Setting up a sine excitation source of 0.2 A at 50 Hz:

-->BODE.INJECTPOINT 1

-->BODE.IAMP 0.2

-->BODE.FREQ 50.0

-->BODE.MODE 2

Related Topics

Using the Performance Servo Tuner on pg. 1

Using the Performance Servo Tuner: Advanced on pg. 1

Scope on pg. 1

Settings on pg. 1

F126 on pg. 1

Error: Invalid Bode plot mode for this function. on pg. 1

BODE.MODE on pg. 1

BODE.INJECTPOINT on pg. 1

BODE.VAMP on pg. 1

BODE.IAMP on pg. 1

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™