You are here: Tools > AKD into KAS > Workbench Reference > BODE.IAMP

BODE.IAMP

General Information

Type

R/W Parameter

Description

Sets current command value used during the Bode procedure.

Units

A

Range

+/- Combined drive and motor current limit

Default Value

0.2 A

Data Type

Float

Start Version

M_01-00-00-000

FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design

Index/Subindex

Object Start Version

EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

5015h/0

M_01-00-00-000

Description

BODE.IAMP sets the amplitude of the excitation when in current mode as set in BODE.INJECTPOINT. When using BODE.MODE on pg. 1 = 1 and BODE.INJECTPOINT on pg. 1 = 1, this parameter will determine the level of noise injected to commanded current value.

Example

Set the excitation current to 0.2 A:

-->BODE.IAMP 0.2

Get the excitation current (already set to 0.2 A):

-->BODE.IAMP 0.200 [A]

Related Topics

Using the Performance Servo Tuner on pg. 1

Using the Performance Servo Tuner: Advanced on pg. 1

Scope on pg. 1

Settings on pg. 1

F126 on pg. 1

Error: Invalid Bode plot mode for this function. on pg. 1

BODE.INJECTPOINT on pg. 1 | BODE.FREQ on pg. 1

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™