You are here: Tools > AKD into KAS > Workbench Reference > BODE.IFTHRESH

BODE.IFTHRESH

General Information

Type

R/W Parameter

Description

Sets the current fault threshold for the BODE.MODE 5 stability test.

Units

A

Range

0.001 to DRV.IPEAK or MOTOR.IPEAK (whichever is lowest) A

Default Value

0 A

Data Type

Decimal

Start Version

M_01-02-10-000

Description

When BODE.MODE on pg. 1 is set to 5, the firmware monitors the drive current (IL.CMD on pg. 1). When IL.CMD goes above BODE.IFTHRESH, an internal counter records the length of time IL.CMD was above BODE.IFTHRESH. If the internal counter reaches BODE.IFLIMIT on pg. 1, Fault 133 (Instability during Autotune) is generated.

Example

Set BODE.IFTHRESH to 6 Amps:

-->BODE.IFTHRESH 6

Set BODE.IFLIMIT to 0.500 seconds:

-->BODE.IFLIMIT 0.5

Set BODE.MODE to 5 to enable stability detection:

BODE.MODE 5

Related Topics

Using the Performance Servo Tuner on pg. 1

Using the Performance Servo Tuner: Advanced on pg. 1

F133 on pg. 1

BODE.MODE on pg. 1,BODE.MODETIMER on pg. 1, BODE.VFLIMIT on pg. 1, BODE.VFTHRESH on pg. 1 , BODE.IFLIMIT on pg. 1

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™