|
General Information |
|
|---|---|
|
Type |
NV Parameter |
|
Description |
Enables/disables modulo functionality. |
|
Units |
None |
|
Range |
0 to 1 |
|
Default Value |
0 (DisableRemoval of the ENABLE signal. Disables power stage.) |
|
Data Type |
Integer |
|
Start Version |
M_01-13-00-000 |
Compare functionality is supported on hardware revisions D, DB, DA, and higher depending on the drive type. Check the label on the side of the drive to ensure the AKD meets one of the following requirements.
| AKD Type | Hardware Revision Supported |
|---|---|
| AKD | Revision D or higher |
| PDMM | Revision DB or higher |
| AKD-T-IC"Integrated Circuits" Miniaturized electronic circuits (consisting mainly of semiconductor devices, as well as passive components) that have been manufactured in the surface of a thin substrate of semiconductor material | Revision DA or higher |
| FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design | Index/Subindex | Object Start Version | |
|---|---|---|---|
| 53A6h/0 |
CMP0.MODEN |
M_01-13-00-000 | |
| 53ADh/0 |
CMP1.MODEN |
||
Description
This keyword enables or disables modulo functionality on CMPx.
An error will be generated if CMPx.SOURCE, CMPx.MODBOUND1, CMPx.MODBOUND2, and CMPx.WIDTH are not set prior to enabling CMPx.MODEN. If CMPx.SETPOINT is not set prior to enabling CMPx.MODEN, the compare will trigger at the last set value, or the default value of 0 if the drive has been power cycled .
CMPx.MODEN must be set before CMPx.SETPOINT on pg. 1.
Example
The following example enables modulo for CMP1.
-->CMP1.MODEN 1
Related Topics
|
Copyright © 2015 Kollmorgen™ |
|