You are here: Tools > AKD into KAS > Workbench Reference > CMP0.SETPOINT, CMP1.SETPOINT

CMPx.SETPOINT

General Information

Type

NV Parameter

Description

Sets the value of a Compare setpointSetpoint is the target value that an automatic control system, for example PID controller, will aim to reach.

Units

Units depend on value of CMPx.SOURCE. See table below.

Range

Argument 1: 0 to 7

Argument 2: -9,223,372,036,854,775,808 to 9,223,372,036,854,775,808

Default Value

9,223,372,036,854,775,808

Data Type

Argument 1: Integer

Argument 2: Integer

Start Version

M_01-13-00-000

Units

CMPx.SOURCE Units
0 (FB1) Depends on FB1.PUNIT on pg. 1 or custom units.
1 (FB2) Depends on FB2.PUNIT on pg. 1 or custom units.
2 (FB3) Depends on FB2.PUNIT on pg. 1 or custom units.
3 (PL.FB) Depends on UNIT.PLINEAR or UNIT.PROTARY
Rotary: counts, rad, deg, (custom units), 16-bit counts
Linear: counts, mm, µm, (custom units), 16-bit counts

Compare functionality is supported on hardware revisions D, DB, DA, and higher depending on the drive type. Check the label on the side of the drive to ensure the AKD meets one of the following requirements.

AKD Type Hardware Revision Supported
AKD Revision D or higher
PDMM Revision DB or higher
AKD-T-IC"Integrated Circuits" Miniaturized electronic circuits (consisting mainly of semiconductor devices, as well as passive components) that have been manufactured in the surface of a thin substrate of semiconductor material Revision DA or higher
FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Index/Subindex Object Start Version

EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

34AAh/1 CMP0.SETPOINT 0 M_01-13-00-000
34AAh/2 CMP0.SETPOINT 1
34AAh/3 CMP0.SETPOINT 2
34AAh/4 CMP0.SETPOINT 3
34AAh/5 CMP0.SETPOINT 4
34AAh/6 CMP0.SETPOINT 5
34AAh/7 CMP0.SETPOINT 6
34AAh/8 CMP0.SETPOINT 7

34BAh/1

CMP1.SETPOINT 0

34BAh/2

CMP1.SETPOINT 1

34BAh/3

CMP1.SETPOINT 2

34BAh/4

CMP1.SETPOINT 3

34BAh/5

CMP1.SETPOINT 4

34BAh/6

CMP1.SETPOINT 5

34BAh/7

CMP1.SETPOINT 6

34BAh/8

CMP1.SETPOINT 7

Description

Use this keyword to set the position value for a Compare setpoint. This position value will be compared against a Compare source (CMPx.SOURCE on pg. 1). If they match, an output pulse is generated. A setpoint also requires a width (CMPx.WIDTH on pg. 1) and width type (CMPx.WIDTHTYPE on pg. 1).

A setpoint must be armed (CMPx.ARM on pg. 1) before it is active. If a setpoints value, width, or width type are changed after it has been armed, that setpoint will be automatically disarmed.

Example

The following example sets the value of setpoint 1 to one billion for CMP1.

-->CMP1.SETPOINT 1 1000000000

Related Topics

Compare Engines on pg. 1

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™